JN5179

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5179

2,416 次查看
wupengfei
Contributor II

To put the module into UART programming mode, tie MISO to 0 V while releasing
RESET. This causes the device to read zeros back from the Flash memory during
initialization and, as a result, to enter programming mode. If you are using the module in
conjunction with a serial interface then the signal PGM is available to put the device into
programming mode. To allow this signal to operate correctly from the Flash programming
software.

What is the signal PGM?

0 项奖励
回复
1 回复

2,100 次查看
davidashraf
Contributor V

wupengfei‌ 

I believe that's is the way to enter programming mode 
https://community.nxp.com/thread/460072 

0 项奖励
回复