Is the KW01 sub-GHz SMAC inserting extra bytes into the packet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the KW01 sub-GHz SMAC inserting extra bytes into the packet?

5,572 次查看
stronglikebool
Contributor I

Hi,

I am transmitting from a simple loop program that I wrote. I am sending the same packet over and over again using the MRB-KW01 development board. I am receiving the packets using another MRB-KW01 that is running the SMAC graphical user interface (GUI) that came loaded on the rcvr board. The frequency is 915 MHz, bit rate = 4800 bps, OOK, continuous mode. I am sending a packet with a 3-byte preamble, a 4-byte sync word, and 8 bytes of payload. Each payload byte is 0x4F. I am monitoring the received packets with an o'scope on the data & clk outputs on j18, the bit error rate test port, of the rcvr MRB-KW01. I am seeing 4 extra bytes inserted into the packet  right after the adr byte and before the payload bytes. Also 2 bytes are inserted after the payload and before the CRC byes. Please see attached jpgs. Might anyone know why these mystery bytes (marked with ? marks) are there? Thank you.

标签 (1)
0 项奖励
回复
1 回复

5,361 次查看
luisburgos
NXP Employee
NXP Employee

Hi Brant,

No, SMAC doesn´t insert extra bytes in the packet.

Could you please verify if this behavior is also reproduced with a bit rate = 50000 bps, FSK modulation and packet mode?

Best regards,

Burgos.

0 项奖励
回复