I want PWM sample code (SMAC codbase) for MC1322x. Please help me.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I want PWM sample code (SMAC codbase) for MC1322x. Please help me.

2,123 次查看
charnonpoolsin
Contributor I

I want PWM sample code (SMAC codbase) for MC1322x. Please help me.

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

1,961 次查看
AngelC
Senior Contributor I

Dear Charnon,

An easy and fast way to learn how to use the Timer module and the TMR drivers described in 22xDRVRRM is to check the BuzzerInit() function inside the Sound.c file of your project. The Buzzer configures the timer module to generate interrupts.

I am also sending you an example code I wrote some time ago using the SMAC Generic App. This code implements the TMR drivers of the MC1322x MCU and their basic functionality. The program starts a timer that toggles its output (PIN 1 in SRB) every 100 ms and enters a callback function every time the counter is reached (every 100 ms). Feel free to use it as an example for your implementation.

Please refer to the timer configuration example for fixed-frequency PWM mode of the timer mode included in the MC1322x Reference manual- chapter 12.7.11 Fixed-Frequency PWM Mode. There are many other configuration examples you may use too.

MC1322xRM: http://cache.freescale.com/files/rf_if/doc/ref_manual/MC1322xRM.pdf

Regards,

AngelC

0 项奖励
回复