How to return to ota_client or how to reload code through ota with KW38?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to return to ota_client or how to reload code through ota with KW38?

1,230 Views
Ingm
Contributor I

hello
I am using the KW38 bluethoot module
use the example codes _bootloader_ota and ota_client_att
and the glucose_sensor_bm example
I followed the steps mentioned in this link


https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Reprogramming-a-KW38-device-using-...


everything works well
but now I want to know how to return the stack of the ota_client code example? to load any code through ota several times

I don't want to start the first steps mentioned in that link... I want to reload code through ota after loading the glucose_sensor_bm or wireless_uart codes examples, or any code but not in a wired way

0 Kudos
Reply
1 Reply

1,204 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well.

I would recommend you checking this Application Note: KW38 - Integrating the OTAP Client Service into a Bluetooth LE Peripheral Device Application Note (n...

You would need to implement some changes on the SDK example, to integrate OTAP feature.

Hope this helps.

 

Regards,

Ricardo

0 Kudos
Reply