How to implement otap server into android app?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to implement otap server into android app?

4,170件の閲覧回数
mangramarco
Contributor III

Hello, i need to develop a android app able to send new firmware to otap client device. There is a documentation? my device has kw41z mcu and it works with iot toolbox.
Thank you

0 件の賞賛
返信
4 返答(返信)

4,149件の閲覧回数
mangramarco
Contributor III

hello, thank you for the reply.

i read the Bluetooth Low Energy application developer guide and i not found any section for android implementation. Furthermore not all informations are clear. For example, i don't understand the correlation between srec records and image file format: S0 record contains the name of file and S2 records tlv byte not correspond in my srec files. I can't find the information displayed into iot toolbox Like "File  name" or "File version". Why file version is hex value?

 

 

Screenshot_2021-09-15-12-39-21-49_f80120ae6db814e228d2c144b4a575a9[1].jpgScreenshot_2021-09-15-12-39-21-49_f80120ae6db814e228d2c144b4a575a9[1].jpg

0 件の賞賛
返信

4,138件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The document describe the OTAP protocol. You need this to develop your APP. Of course, it doesn't have the description about how to develop APP.  

You can also refer this article. This article tells you about the OAT header. The file name and file version is included in OTA header. When you use iot tool box, if your image doesn't have the OTA header, the iot toolbox will add this for you. If you want to set the ota header by yourself. You can use the test tool.

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

4,129件の閲覧回数
mangramarco
Contributor III

 if your image doesn't have the OTA header, the iot toolbox will add this for you

 

thank you!!!

0 件の賞賛
返信

4,161件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

 

Please download the kw36 sdk. It has many useful document about the ble development.

In directory 'docs\wireless\Bluetooth', the 'Bluetooth Low Energy Application Developer Guide' introduce the otap. You can also refer this link 

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信