How to get ZDP cluster message and low power mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get ZDP cluster message and low power mode

1,770 次查看
leoxie
Contributor I

Dear everyone,

I have a some question,Would you help me,thanks in advance.

Chip:JN5169

Stack:JN-AN-1189

1、how could I get the ZDP cluster callback or message in application layer,

for example, I want to get these cluser message in application layer,So I try to collect stack event,but it's didn't work...

#define ZDP_NWK_ADDR_RSP_CLUSTER_ID (0x8000)
#define ZDP_IEEE_ADDR_RSP_CLUSTER_ID (0x8001)
#define ZDP_NODE_DESC_RSP_CLUSTER_ID (0x8002)
#define ZDP_POWER_DESC_RSP_CLUSTER_ID (0x8003)
#define ZDP_SIMPLE_DESC_RSP_CLUSTER_ID (0x8004)
#define ZDP_ACTIVE_EP_RSP_CLUSTER_ID (0x8005)
#define ZDP_MATCH_DESC_RSP_CLUSTER_ID (0x8006)
#define ZDP_COMPLEX_DESC_RSP_CLUSTER_ID (0x8010)
#define ZDP_USER_DESC_RSP_CLUSTER_ID (0x8011)

the code:

/* Collect stack Events */
else if ( OS_eCollectMessage(APP_msgZpsEvents, &sStackEvent) == OS_E_OK)
{

// when I gateway send some ZDP cluster req, It's can't come over here.
DBG_vPrintf(TRACE_OUTLET_NODE, "Stack Event type: %d\n", sStackEvent.eType);

/*Request response event, call the child age logic */
if((ZPS_EVENT_APS_DATA_INDICATION == sStackEvent.eType) &&
(0 == sStackEvent.uEvent.sApsDataIndEvent.u8DstEndpoint ))
{

ZPS_tsAfZdpEvent sAfZdpEvent;
zps_bAplZdpUnpackResponse(&sStackEvent,&sAfZdpEvent);

DBG_vPrintf(TRACE_OUTLET_NODE, "APP: vCheckStackEvent: ZPS_EVENT_APS_ZDP_REQUEST_RESPONSE, Cluster = %x\n", sAfZdpEvent.u16ClusterId );

if (ZDP_MATCH_DESC_RSP_CLUSTER_ID == sAfZdpEvent.u16ClusterId)
{
DBG_vPrintf(TRACE_OUTLET_NODE,"APP_MATCH_DESCRIPTOR_RESPONSE..");

}

if (ZDP_ACTIVE_EP_REQ_CLUSTER_ID == sAfZdpEvent.u16ClusterId)
{
DBG_vPrintf(TRACE_OUTLET_NODE,"ZDP_ACTIVE_EP_REQ_CLUSTER_ID..");
}

if (ZDP_MGMT_PERMIT_JOINING_REQ_CLUSTER_ID == sAfZdpEvent.u16ClusterId)
{
DBG_vPrintf(TRACE_OUTLET_NODE,"ZDP_DISCOVERY_CACHE_RSP_CLUSTER_ID..");
}

.................. do the same as above


}
}

2、When dose the end-device should into sleep.

The HA stack seem to must stop all timer before into sleep mode,but what time the decive should into sleep mode after device awake.

I try to decrease APP_PollTimer and APP_TickTimer period and set KEEPALIVETIME=20,but when the gateway is power down( no other router ),the device can't find the network vanish and get on/off command from gateway. 

Best Regards,

Leo

QQ:2442926161

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,435 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Leo,

Check the structure  ZPS_teAfEventType, print that value, you are not getting a successful event.

I recommended to you check the app_event_handl.c file.

- You can go into sleep mode if you do not have an event.

- Stop the poll timer,the device to go back to sleep.

Hope it helps.

Best Regards,

Mario

0 项奖励
回复