How to change file version of Ota file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change file version of Ota file

ソリューションへジャンプ
1,562件の閲覧回数
yuboli
Contributor II

Hi  every one,

   I compiled externalized ColorLight with JN-AN-1218. I want to change the version of Ota file and how to modify it.

D7J]Y{C[0ZQLG[IU]4Y15]8.png

0 件の賞賛
返信
1 解決策
1,466件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

Could you please take a look at this document here? Appendix B has some related information to the values related to OTA version.

 

The example provided in said document is for a null OTA file, but the concept applies to regular OTA files as well.

As you can see in the image below, the first two bytes correspond to Manufacturer code, then two bytes for image type, and one byte for version number, followed by 3 "zero" bytes.

 

pastedImage_2.png

 

You can also change the version number using JET, as explained in section 3.3 of the same document.

 

Please let me know if you need more information.

 

Best regards,

Sebastian

元の投稿で解決策を見る

1 返信
1,467件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

Could you please take a look at this document here? Appendix B has some related information to the values related to OTA version.

 

The example provided in said document is for a null OTA file, but the concept applies to regular OTA files as well.

As you can see in the image below, the first two bytes correspond to Manufacturer code, then two bytes for image type, and one byte for version number, followed by 3 "zero" bytes.

 

pastedImage_2.png

 

You can also change the version number using JET, as explained in section 3.3 of the same document.

 

Please let me know if you need more information.

 

Best regards,

Sebastian