How to change file version of Ota file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change file version of Ota file

Jump to solution
1,551 Views
yuboli
Contributor II

Hi  every one,

   I compiled externalized ColorLight with JN-AN-1218. I want to change the version of Ota file and how to modify it.

D7J]Y{C[0ZQLG[IU]4Y15]8.png

0 Kudos
Reply
1 Solution
1,455 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

Could you please take a look at this document here? Appendix B has some related information to the values related to OTA version.

 

The example provided in said document is for a null OTA file, but the concept applies to regular OTA files as well.

As you can see in the image below, the first two bytes correspond to Manufacturer code, then two bytes for image type, and one byte for version number, followed by 3 "zero" bytes.

 

pastedImage_2.png

 

You can also change the version number using JET, as explained in section 3.3 of the same document.

 

Please let me know if you need more information.

 

Best regards,

Sebastian

View solution in original post

1 Reply
1,456 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

Could you please take a look at this document here? Appendix B has some related information to the values related to OTA version.

 

The example provided in said document is for a null OTA file, but the concept applies to regular OTA files as well.

As you can see in the image below, the first two bytes correspond to Manufacturer code, then two bytes for image type, and one byte for version number, followed by 3 "zero" bytes.

 

pastedImage_2.png

 

You can also change the version number using JET, as explained in section 3.3 of the same document.

 

Please let me know if you need more information.

 

Best regards,

Sebastian