How do I read/write to an ISO15693 tag using NXP NFC Cockpit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I read/write to an ISO15693 tag using NXP NFC Cockpit?

5,639件の閲覧回数
alexpainter3
Contributor I

Hi,

I'm using the NFC cockpit v4.8.0 to work with HF RFID tags using the ISO15693 protocol. I'm able to send data to a ISO14443A tag I have and receive bytes back, but when I try to use my ISO 15693 tag, I'm not able to write data to this card (ERROR:RFProtocolType15693Service:Perform15693DataExchangeFailed) or read blocks (ERROR:RFProtocolType15693Service:PerformReadSingleBlockFailed). I'm able to get the tag's UID through the Inventory button but reading and writing always throws these errors. Any advice would be great!

pastedImage_391.png

タグ(3)
0 件の賞賛
返信
1 返信

5,265件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

According to the image, I assume you are working with CLRC663 eval board. Regarding the Tag, did you make sure that the Tag's block you are trying to read is not password protected or require authentication?

BR,

Ivan.

0 件の賞賛
返信