How do I read/write to an ISO15693 tag using NXP NFC Cockpit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I read/write to an ISO15693 tag using NXP NFC Cockpit?

5,708 Views
alexpainter3
Contributor I

Hi,

I'm using the NFC cockpit v4.8.0 to work with HF RFID tags using the ISO15693 protocol. I'm able to send data to a ISO14443A tag I have and receive bytes back, but when I try to use my ISO 15693 tag, I'm not able to write data to this card (ERROR:RFProtocolType15693Service:Perform15693DataExchangeFailed) or read blocks (ERROR:RFProtocolType15693Service:PerformReadSingleBlockFailed). I'm able to get the tag's UID through the Inventory button but reading and writing always throws these errors. Any advice would be great!

pastedImage_391.png

0 Kudos
Reply
1 Reply

5,334 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

According to the image, I assume you are working with CLRC663 eval board. Regarding the Tag, did you make sure that the Tag's block you are trying to read is not password protected or require authentication?

BR,

Ivan.

0 Kudos
Reply