Getting MAC-Address from Framework on FRDM-KW41Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting MAC-Address from Framework on FRDM-KW41Z

2,554件の閲覧回数
steffenjahnkepa
Contributor III

Hello,

i am using the FREEDOM-KW41Z with the frdmkw41z_wireless_examples_thread_router_eligible_device_freertos Example and for one of my applications i need to get the MAC-Address of this Device in the network, to get an unique ID for this board. Any Ideas where to find this address or the function to build it? Thanks a lot!

Best Regards,

Steffen

ラベル(3)
3 返答(返信)

2,174件の閲覧回数
steffenjahnkepa
Contributor III

Hello estephania_martinez

this works fine for the THREAD examples! But i can't find an EUI or MAC that i could use for my application if I'm using the SDK-Examples wireless examples > bluetoth > ipv6_node and wireless examples > bluetoth > ipv6_router. Or am I wrong?

Best Regards,

Steffen

0 件の賞賛
返信

2,174件の閲覧回数
steffenjahnkepa
Contributor III

I got it. :smileywink:

It is the eui. you can get this address with thr get eui in the shell.

2,174件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

You are right the eui Extended Unique Identifier it's the information you need.

Best Regards, 

Estephania 

0 件の賞賛
返信