Getting MAC-Address from Framework on FRDM-KW41Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting MAC-Address from Framework on FRDM-KW41Z

2,555 次查看
steffenjahnkepa
Contributor III

Hello,

i am using the FREEDOM-KW41Z with the frdmkw41z_wireless_examples_thread_router_eligible_device_freertos Example and for one of my applications i need to get the MAC-Address of this Device in the network, to get an unique ID for this board. Any Ideas where to find this address or the function to build it? Thanks a lot!

Best Regards,

Steffen

标签 (3)
3 回复数

2,175 次查看
steffenjahnkepa
Contributor III

Hello estephania_martinez

this works fine for the THREAD examples! But i can't find an EUI or MAC that i could use for my application if I'm using the SDK-Examples wireless examples > bluetoth > ipv6_node and wireless examples > bluetoth > ipv6_router. Or am I wrong?

Best Regards,

Steffen

0 项奖励
回复

2,175 次查看
steffenjahnkepa
Contributor III

I got it. :smileywink:

It is the eui. you can get this address with thr get eui in the shell.

2,175 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

You are right the eui Extended Unique Identifier it's the information you need.

Best Regards, 

Estephania 

0 项奖励
回复