For Zigbee Pro stack what is the maximum achievable throughput?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For Zigbee Pro stack what is the maximum achievable throughput?

4,607 Views
harshadamodak
Contributor I

For Zigbee Pro stack what is the maximum achievable throughput?

As the bandwidth is 250 kbps, what is maximum throughput achievable?

We are trying to check if one node is network is able to send 38.4 kbps data on Zigbee Pro network.

4 Replies

4,004 Views
karel_povalac
NXP Employee
NXP Employee

Definitely a number of hops influence the maximum throughput. Our experience for example with the wireless UART application was achieving stable baudrate 38400bps. However, many factors can affect the communication speed on particular Zigbee channel.

4,004 Views
alanled
Contributor II

Hello Karel !!! :smileyhappy: It's good to see you are still nailing solutions at NXP. I send you a big hug.

0 Kudos
Reply

4,004 Views
karel_povalac
NXP Employee
NXP Employee

Hi Alan, ​good to hear about you as well :smileyhappy:. You still have a lot experiences with Zigbee... Hey, let's make a chat on private thread.

0 Kudos
Reply

4,004 Views
alanled
Contributor II

It depends on how many hops it has to go through the network, if you need APS acknowledgement, if the channel is busy, then retries at MAC level will happen, etc. So Rule of thumb, you should expect 10ms of latency per hop. This is my experience from building real Zigbee applications.