For Zigbee Pro stack what is the maximum achievable throughput?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For Zigbee Pro stack what is the maximum achievable throughput?

4,597件の閲覧回数
harshadamodak
Contributor I

For Zigbee Pro stack what is the maximum achievable throughput?

As the bandwidth is 250 kbps, what is maximum throughput achievable?

We are trying to check if one node is network is able to send 38.4 kbps data on Zigbee Pro network.

4 返答(返信)

3,994件の閲覧回数
karel_povalac
NXP Employee
NXP Employee

Definitely a number of hops influence the maximum throughput. Our experience for example with the wireless UART application was achieving stable baudrate 38400bps. However, many factors can affect the communication speed on particular Zigbee channel.

3,994件の閲覧回数
alanled
Contributor II

Hello Karel !!! :smileyhappy: It's good to see you are still nailing solutions at NXP. I send you a big hug.

0 件の賞賛
返信

3,994件の閲覧回数
karel_povalac
NXP Employee
NXP Employee

Hi Alan, ​good to hear about you as well :smileyhappy:. You still have a lot experiences with Zigbee... Hey, let's make a chat on private thread.

0 件の賞賛
返信

3,994件の閲覧回数
alanled
Contributor II

It depends on how many hops it has to go through the network, if you need APS acknowledgement, if the channel is busy, then retries at MAC level will happen, etc. So Rule of thumb, you should expect 10ms of latency per hop. This is my experience from building real Zigbee applications.