End device with automatic wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

End device with automatic wake up

2,832 Views
raheleh
Contributor II

Which one of the zigbee demo applications from beekit demonstrates an end device that automatically wakes up from Doze or Hibernate based on internal timeouts or clock ticks?

we have an end device with scheduled automatic wake up but it misses the wake up every once in a while. 

Thanks!

0 Kudos
Reply
2 Replies

2,636 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Raheleh,

As you know the beekit is the old version for the zigbee stack. 

Could you please take a look for the Beestack 5.0.0?

https://www.nxp.com/webapp/Download?colCode=KINETIS-BEESTACK&appType=license&location=null&fsrch=1&s... 

Hope it helps

Let me know if you have problems with the examples

Mario

0 Kudos
Reply

2,636 Views
raheleh
Contributor II

Hi Mario, 

we have to troubleshoot this problem for our existing MC13226 based devices.

so i don`t think referring to the kinetis series helps. 

there must be examples on the old beekit as well for sleepy devices. let me know please if you are aware of them. 

thanks!

0 Kudos
Reply