Different versions of the protocol stack device connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Different versions of the protocol stack device connection

1,489 次查看
18341265598
Contributor II

Hi everyone:

    I have two different devices, coordinate and end device. coordinate is zigbee 3.0 base device application note and end device is zigbee HA demo's ColorDimmerSwitch,respectively as follow:

pastedImage_1.pngpastedImage_3.png

    Now i want to establish link between coordinate and end device,but i failed.

    Note:These two devices use different protocol stacks

    Can you give me some tips or ideas? thank you!!!

    

标记 (1)
0 项奖励
回复
2 回复数

1,428 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Zhang, I hope you're doing well!

 

The Zigbee 3.0 stack and the Zigbee HA stack are compatible, so you should be able to work with a Zigbee 3.0 Base device and your HA end device.

 

The ColorDimmerSwitch device is acting as a commissioner of the light devices, so it can control them.

May I ask, what is your final application? If the ColorDimmerSwitch is not working out for you, I would recommend you to try with the ColorSceneController instead, included in the JN-AN-1219 application note.

 

Please let me know if you have any further questions.

 

Best regards,

Sebastian

0 项奖励
回复

1,428 次查看
18341265598
Contributor II

Hi Sebastian,

    As you said, the Zigbee 3.0 Base device works with HA end device well.

    I just want to control an HA OnOff  end device,now it works well.

    Thanks you.

0 项奖励
回复