Couldn't run MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Couldn't run MCUXpresso IDE

ソリューションへジャンプ
2,547件の閲覧回数
sChameleoNz
Contributor III

I'm using MCUXpresso IDE v11.4.0.6224.

I installed SDK_2_6_3_JN5189DK6.

The tool works well in this point.

Next, I installed the Zigbee Configuration Editor plug-in.

And, I couldn't run the tool.

When I try to run the MCUXpresso IDE, the tool is automatically closed when it is opening.

I tried reinstall the tool after cleaning, 10 times, but it was the same every single time.

How do I use the MCUXpresso IDE with Zigbee Configuration Editor?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,534件の閲覧回数
sChameleoNz
Contributor III

Self-Answered

It needs JRE.

元の投稿で解決策を見る

1 返信
2,535件の閲覧回数
sChameleoNz
Contributor III

Self-Answered

It needs JRE.