Couldn't run MCUXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Couldn't run MCUXpresso IDE

跳至解决方案
2,582 次查看
sChameleoNz
Contributor III

I'm using MCUXpresso IDE v11.4.0.6224.

I installed SDK_2_6_3_JN5189DK6.

The tool works well in this point.

Next, I installed the Zigbee Configuration Editor plug-in.

And, I couldn't run the tool.

When I try to run the MCUXpresso IDE, the tool is automatically closed when it is opening.

I tried reinstall the tool after cleaning, 10 times, but it was the same every single time.

How do I use the MCUXpresso IDE with Zigbee Configuration Editor?

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
2,569 次查看
sChameleoNz
Contributor III

Self-Answered

It needs JRE.

在原帖中查看解决方案

1 回复
2,570 次查看
sChameleoNz
Contributor III

Self-Answered

It needs JRE.