Configuring multiple temperature sensors using FRDM-KW36

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring multiple temperature sensors using FRDM-KW36

Jump to solution
1,189 Views
SeokJin
Contributor II

Hello.

I am currently learning about BLE communication using the FRDM-KW36 board and KW36 SDK.

-> For reference, the MCUXpresso version is 'v11.8.1_1197' and the KW36 SDK version is 'SDK_2_2_12_FRDM-KW36'!

 

Currently, I am learning based on the example “5.14 Low Power Temperature Sensor and Collector” in the Bluetooth® Low Energy Demo Applications User’s Guide, but I am stuck and am asking a question.

In this example, it consists of one temp sensor (Server device) and one temp collector (Client device), and it was confirmed that the sensor measures the temperature and passes it to the collector through BLE communication.

 

The question here is, can more than 2 temp sensors (Server devices) be connected to one temp collector (Client device)??

I would like to implement a system in which 2 to 3 temp sensors are connected to one temp collector and transmit the temperature through BLE communication. Is it possible??

If possible, please let me know how to configure it!

 

I'm waiting for your reply. Thanks in advance.

Regards,

SeokJin.

Labels (1)
0 Kudos
Reply
1 Solution
1,139 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello SeokJin,

 

Hope you are doing well. Yes, it can be achieved. But, it would be a custom profile.

Please refer to: KW38 Custom Profile - NXP Community

Also, you might want to check the Wireless UART example, as it already supports multiple connections.

 

Hope this helps!

 

Regards,

Ricardo

View solution in original post

0 Kudos
Reply
1 Reply
1,140 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello SeokJin,

 

Hope you are doing well. Yes, it can be achieved. But, it would be a custom profile.

Please refer to: KW38 Custom Profile - NXP Community

Also, you might want to check the Wireless UART example, as it already supports multiple connections.

 

Hope this helps!

 

Regards,

Ricardo

0 Kudos
Reply