Can NXP Bluetooth communicate with TI Bluetooth?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can NXP Bluetooth communicate with TI Bluetooth?

1,478件の閲覧回数
STDUYMAN
Contributor I
0 件の賞賛
返信
1 返信

1,460件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi, I hope you're doing well!

 

NXP products support a variety of Wireless Communications Protocols, like Bluetooth Low Energy, Bluetooth Classic, Wi-Fi, ZigBee, Thread, among others. Depending on the family and device, some devices support different combinations of these protocols, but all of them adhere to their corresponding specification.

 

In the case of the Bluetooth Low Energy devices, like the KW38 family of MCUs, the Bluetooth Low Energy stack they run was designed to comply with Bluetooth Core Specification V5.0, which allows for connection with other devices adhering to the Bluetooth Core Specification.

 

Please let me know if you need any more information about a specific device.

 

Best regards,

Sebastián

0 件の賞賛
返信