Can JN5169 externally expand RAM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can JN5169 externally expand RAM?

1,657件の閲覧回数
1979717461
Contributor III

Can JN5169 externally expand RAM? I want to confirm whether JN5169 can expand RAM.

If you know, tell me.

Thanks!

ラベル(1)
  • JN

タグ(2)
0 件の賞賛
返信
1 返信

1,595件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi, I hope you're doing well!

 

Theoretically speaking, it's possible to add external RAM, because the JN5169's memory map has unassigned address blocks, but the included APIs don’t natively support external RAM. To do this, you would have to implement it yourself. Alternatively, you could try using an external flash or EEPROM memory instead of RAM.

 

Please let me know if you need more information.

 

Best regards,

Sebastian

0 件の賞賛
返信