Can JN5169 externally expand RAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can JN5169 externally expand RAM?

1,659 Views
1979717461
Contributor III

Can JN5169 externally expand RAM? I want to confirm whether JN5169 can expand RAM.

If you know, tell me.

Thanks!

Labels (1)
  • JN

Tags (2)
0 Kudos
Reply
1 Reply

1,597 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi, I hope you're doing well!

 

Theoretically speaking, it's possible to add external RAM, because the JN5169's memory map has unassigned address blocks, but the included APIs don’t natively support external RAM. To do this, you would have to implement it yourself. Alternatively, you could try using an external flash or EEPROM memory instead of RAM.

 

Please let me know if you need more information.

 

Best regards,

Sebastian

0 Kudos
Reply