CLEV6630B firmware and code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLEV6630B firmware and code

5,308件の閲覧回数
eric_wanghao
Contributor I
Hello,
I'm Eric.For some reason,I need OM26630FDK default firmware to debug my
CLEV6630B  board.Where can I download firmware and  source code?
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,978件の閲覧回数
firmsol
Contributor II

Hi eric_wanghao

I want to interface external STM32g series MCU to CLRC663 chip of CLEV6630B eval board.
I am trying to read version register but the CLRC chip is not responding at all.

1) Do we need any configurations for CLRC registers to read version register.
2) I have removed the resistors to bypass the onboard LPC controller also.


do you have any insights for this?

0 件の賞賛
返信

5,109件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Flashing the firmware will be required to work with NFC Cockpit as mentioned in chapter 3.1 of AN11022. On the other hand, for development, it will be enough to import the NFC Reader Library to MCUXpresso and flash a software example.

Hope this helps.

Regards,

Ivan.

0 件の賞賛
返信