CLEV6630B firmware and code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLEV6630B firmware and code

5,303 Views
eric_wanghao
Contributor I
Hello,
I'm Eric.For some reason,I need OM26630FDK default firmware to debug my
CLEV6630B  board.Where can I download firmware and  source code?
Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,973 Views
firmsol
Contributor II

Hi eric_wanghao

I want to interface external STM32g series MCU to CLRC663 chip of CLEV6630B eval board.
I am trying to read version register but the CLRC chip is not responding at all.

1) Do we need any configurations for CLRC registers to read version register.
2) I have removed the resistors to bypass the onboard LPC controller also.


do you have any insights for this?

0 Kudos
Reply

5,104 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Flashing the firmware will be required to work with NFC Cockpit as mentioned in chapter 3.1 of AN11022. On the other hand, for development, it will be enough to import the NFC Reader Library to MCUXpresso and flash a software example.

Hope this helps.

Regards,

Ivan.

0 Kudos
Reply