!!! Bus error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

!!! Bus error

5,673件の閲覧回数
quanjunzhang
Contributor III

Recently,I want to read and write the external FLASH on the carrier board.

HERE, I only print one variable,An “!!! Bus error”  error occurred。

What could be causing this error?

Thanks very much.

Application Notes:JN-AN-1217-Zigbee-3-0-Base-Device

4 返答(返信)

5,526件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Zhang,

As you know, the JN-AN-1217 doesn´t have implemented the read flash process.

You can look at the JN-AN-1220 and follow the external flash implementation. app_ota_client.c file

Regards,

Mario

5,526件の閲覧回数
quanjunzhang
Contributor III

Hi Mario,

 it's OK now. thank you very much for your help.

Regards,

Zhang

5,526件の閲覧回数
quanjunzhang
Contributor III

flash.PNG

0 件の賞賛
返信

5,525件の閲覧回数
quanjunzhang
Contributor III

flash1.PNG

0 件の賞賛
返信