!!! Bus error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

!!! Bus error

6,095 次查看
quanjunzhang
Contributor III

Recently,I want to read and write the external FLASH on the carrier board.

HERE, I only print one variable,An “!!! Bus error”  error occurred。

What could be causing this error?

Thanks very much.

Application Notes:JN-AN-1217-Zigbee-3-0-Base-Device

4 回复数

5,948 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Zhang,

As you know, the JN-AN-1217 doesn´t have implemented the read flash process.

You can look at the JN-AN-1220 and follow the external flash implementation. app_ota_client.c file

Regards,

Mario

5,948 次查看
quanjunzhang
Contributor III

Hi Mario,

 it's OK now. thank you very much for your help.

Regards,

Zhang

5,948 次查看
quanjunzhang
Contributor III

flash.PNG

0 项奖励
回复

5,947 次查看
quanjunzhang
Contributor III

flash1.PNG

0 项奖励
回复