Bug report: Zigbee SDK uses endpoint indices instead of IDs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bug report: Zigbee SDK uses endpoint indices instead of IDs

597 次查看
dstevens
Contributor II

The BDB functions BDB_vFbExitAsTarget and BDB_vFbExitAsTarget in the bcb_fb_target.c SDK source incorrectly treat the provided endpoint parameter as a 1-based index rather than and endpoint ID:

BDB_vFbExitAsTarget

  • Calls eZCL_WriteLocalAttributeValue, which requires an ID, not an index
  • Updates local state with: aeFBState[u8SourceEndpoint - 1] = E_FB_IDLE_STATE, which requires a 1-based index.

 

BDB_eFbTriggerAsTarget expects a 1-based index

  • Returns an error if u8Endpoint > BDB_FB_NUMBER_OF_ENDPOINTS
  • As with the previous function, it calls eZCL_WriteLocalAttributeValue which requires an ID, and then udpates aeFBState assuming a 1-based index (aeFBState[u8EndPoint - 1] = E_FB_IN_PROGRESS_STATE).

 

These bugs are hidden when endpoint IDs are contiguous and begin at 1, which is the case in the samples.

FYI, we previously reported a similar bug in the OTA code here.

SDK Version: 2.6.15

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

562 次查看
sofiaurueta
NXP Employee
NXP Employee

Hello,

 

Thank you for your feedback, let me check this internally with the responsible team.

 

Regards,

Ana Sofia.

0 项奖励
回复