BeyondStudio for NXP, problem with duplicate paths

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BeyondStudio for NXP, problem with duplicate paths

ソリューションへジャンプ
8,535件の閲覧回数
ffonck96
Contributor II

Hi y'all.

I just imported a project for my JN5168 and i'm getting this error message when compiling:

 

 

Description	Resource	Path	Location	Type
Invalid project path: Duplicate path entries found (/nd007-firmware [Include path] isSystemInclude:true includePath:C:/NXP/bstudio_nxp/sdk/JN-SW-4170/Components/Common/Include), path: [/nd007-firmware].	nd007-firmware		pathentry	Path Entry Problem

 

 

Does anyone knows how to fix this problem? I tried to find the "isSystemInclude" property but no results.

Best Regards!

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
8,470件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Please, open the Project properties and go to C/C++ General (left side of Properties window) > Paths and Symbols.

EduardoZamora_0-1700082886906.pngEduardoZamora_0-1700082886906.png

In Includes tab, look for the directory that can be causing the duplicate warning (or any other duplicated directories) and try deleting it.

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
11 返答(返信)
8,516件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @ffonck96

Hope you are doing well.

This behavior may be related to Eclipse. Could you please confirm that you have followed the BeyondStudio User Guide to import and build the project?

By any chance, did you rename the project or perhaps delete and reimport the project?

Regards,
Eduardo.

0 件の賞賛
返信
8,507件の閲覧回数
ffonck96
Contributor II

Hi @EduardoZamora Thanks again for your quick reply. You have been very helpful.

  • This behavior may be related to Eclipse. Could you please confirm that you have followed the BeyondStudio User Guide to import and build the project?

Now i'm following the instructions step by step on the document you provided me, but i still have the issue.
The sequence of things i did is as follows:

  1. Open BeyondStudio and set workspace on path: C:\NXP\bstudio_nxp\workspace
  2. Import project into workspace. Select the code and import.
  3. Clean the project just in case. Then build the application. Build finishes with 31 Warnings. One of them is what i explained before: "Invalid project path: Duplicate path entries found...."
  • By any chance, did you rename the project or perhaps delete and reimport the project?

Precisely i copy-pasted this code from another computer's coworker. In other words, i copy-pasted the folder.

Regards!

0 件の賞賛
返信
8,497件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Please, try the following procedure:

  1. Delete all possible previous versions of the project you are trying to import

  2. Copy the folder (not a zip) that contains the project and paste it into C:\NXP\bstudio_nxp\workspace

  3. Follow the menu path File > Import

  4. Expand General and select Existing Projects into Workspace

  5. In the dialogue, uncheck Copy projects into workspace option

  6. Select "Select root directory" and browse for the folder you copied into C:\NXP\bstudio_nxp\workspace (step 1)

  7. Click on Finish

After this, try building your project. Please, let me know your findings.

Regards,
Eduardo.

0 件の賞賛
返信
8,476件の閲覧回数
ffonck96
Contributor II

Hi @EduardoZamora .

I did the precedure as you mentioned and i still have the warning.

By the way the tree of the folder is as following:

workspace/
└── nd007-firmware
    ├── Common
    │   └── Source
    ├── SleepingEndDevice
    │   ├── Build
    │   └── Source
    └── img

I attached a photo with the warning I'm mentioning.

ffonck96_0-1700072502633.pngffonck96_0-1700072502633.png

Regards.

0 件の賞賛
返信
8,471件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Please, open the Project properties and go to C/C++ General (left side of Properties window) > Paths and Symbols.

EduardoZamora_0-1700082886906.pngEduardoZamora_0-1700082886906.png

In Includes tab, look for the directory that can be causing the duplicate warning (or any other duplicated directories) and try deleting it.

Regards,
Eduardo.

0 件の賞賛
返信
8,460件の閲覧回数
ffonck96
Contributor II

Hi @EduardoZamora .

You were right about the duplicate paths. I had like 10 duplicate paths and 3 symbols too.

ffonck96_0-1700141958577.pngffonck96_0-1700141958577.png

Now it can compile without having the duplicate path problem. However, several errors and new warnings are visible.

ffonck96_1-1700142283431.pngffonck96_1-1700142283431.png

I want to know if there's another way to make this work or am i missing something?

Regards!

0 件の賞賛
返信
8,446件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Could you please confirm that you have followed BeyondStudio for NXP Installation and User Guide, Section 2.1 Creating a Workspace, Step 4 for Workspace preferences configuration?

Also, maybe you can try flushing the indexer; in project's context menu, select Index > Rebuild and Index > Freshen All Files.

EduardoZamora_0-1700149511285.pngEduardoZamora_0-1700149511285.png

Regards,
Eduardo.

0 件の賞賛
返信
8,438件の閲覧回数
ffonck96
Contributor II

Hi @EduardoZamora .

I did your suggest and still have the issue. I just figured it out that BeyondStudio managed to create the .elf/.bin file despite having trouble with errors and warnings. It seems that the IDE lost the references of some variables.

Regards.

0 件の賞賛
返信
8,417件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Please, take a look at the following post: Beyond Studio Common Errors - NXP Community.

Regards,
Eduardo.

0 件の賞賛
返信
8,262件の閲覧回数
ffonck96
Contributor II

hi Eduardo.

I checked the document and didnt find any related Error regarding my problem.

As you mentioned, the project I have wasn't properly copied from another enviroment and maybe there're some configurations messing around.

Also, i haven't downloaded the JenOS plugin, since the only one i found so far was the "ZPS Configuration Editor". Idk if this has an impact in the compilation process.

 

What gives?

0 件の賞賛
返信
8,249件の閲覧回数
ffonck96
Contributor II
At the end all ended up being bad code from the author of the code. I really appreciate all the help u gave me.

Regards!