BLE Carrier Wave and Modulation options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE Carrier Wave and Modulation options

ソリューションへジャンプ
3,061件の閲覧回数
alexishernandez
Contributor III

Hi community, i'm using the MKW40 BLE Module and i want to know if there is any way to enable/disable the modulation, enable/disable the radio and the carrier wave without modulation.

From the KW40Zxx Reference Manual :

Chapter 44: Use of the radio will be facilitated through firmware provided by Freescale giving
customers access to all the radio features through appropriate API interfaces. As such,
detailed information on radio control registers is not provided here.
Where are those appropriate API interfaces?
Best regards.

ラベル(3)
1 解決策
2,672件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alexis Hernandez

Please check the followings community posts:

NXP connectivity FCC/ETSI Certification Software 

https://community.nxp.com/docs/DOC-332721 

There is already examples codes that allows you to test radio in the connectivity software, I recommend you to check them, also please check the code to find out how radio is set.

Hope this information could help you, please let me know if you have any question about this.

Best Regards

Jorge Alcala

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,673件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alexis Hernandez

Please check the followings community posts:

NXP connectivity FCC/ETSI Certification Software 

https://community.nxp.com/docs/DOC-332721 

There is already examples codes that allows you to test radio in the connectivity software, I recommend you to check them, also please check the code to find out how radio is set.

Hope this information could help you, please let me know if you have any question about this.

Best Regards

Jorge Alcala

0 件の賞賛
返信