BLE Carrier Wave and Modulation options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE Carrier Wave and Modulation options

Jump to solution
3,016 Views
alexishernandez
Contributor III

Hi community, i'm using the MKW40 BLE Module and i want to know if there is any way to enable/disable the modulation, enable/disable the radio and the carrier wave without modulation.

From the KW40Zxx Reference Manual :

Chapter 44: Use of the radio will be facilitated through firmware provided by Freescale giving
customers access to all the radio features through appropriate API interfaces. As such,
detailed information on radio control registers is not provided here.
Where are those appropriate API interfaces?
Best regards.

Labels (3)
1 Solution
2,627 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alexis Hernandez

Please check the followings community posts:

NXP connectivity FCC/ETSI Certification Software 

https://community.nxp.com/docs/DOC-332721 

There is already examples codes that allows you to test radio in the connectivity software, I recommend you to check them, also please check the code to find out how radio is set.

Hope this information could help you, please let me know if you have any question about this.

Best Regards

Jorge Alcala

View solution in original post

0 Kudos
Reply
1 Reply
2,628 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alexis Hernandez

Please check the followings community posts:

NXP connectivity FCC/ETSI Certification Software 

https://community.nxp.com/docs/DOC-332721 

There is already examples codes that allows you to test radio in the connectivity software, I recommend you to check them, also please check the code to find out how radio is set.

Hope this information could help you, please let me know if you have any question about this.

Best Regards

Jorge Alcala

0 Kudos
Reply