BGA2869 pcb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BGA2869 pcb

3,008件の閲覧回数
hyd
Contributor I

我正在联系以请求BGA2869的PCB文件。我正在设计一个需要此组件的项目,我将不胜感激在获取必要文件方面的任何帮助。

据我了解,BGA2869是一款高性能射频放大器,设计用于各种应用,包括无线基础设施和广播设备。凭借其高线性度和增益,它是许多RF电路中必不可少的元件。

由于我是恩智浦社区的新成员,我不确定如何获取所需的文件。因此,我希望就如何处理这一请求提供任何指导。

提前感谢您的帮助。

最好的问候,海德

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,991件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @hyd ,

Thanks for contact NXP support. As the DataSheet providing some necessary information for the BGA2869, there isn't direct PCB file for external.

Could you please consult the datasheet to carry out your design? Especially the second chapter(Pinning information) and tenth chapter(Package outline).

Here you can find the datasheet of BGA2869.

 

B.R.

Gavin

0 件の賞賛
返信

2,985件の閲覧回数
hyd
Contributor I

I need to use this chip in my project, but I have no experience in designing high-frequency circuits. Do you have any examples of PCB designs (preferably with PCB design files)?

 
タグ(1)
0 件の賞賛
返信

2,978件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @hyd ,

NXP has some guidance materials on PCB design, which you can download on the website. For example, High Speed Layout Design Guidelines describes general principles of high-speed layout design,PCB design and layout guidelines for CBTU02044 describes PCB design and layout recommendations using the CBTU02044 switch chip, PCB Layout Design for Analog Applications  describes PCB layout design guidelines for analog applications. You can choose the right information to refer to according to your specific needs.

Data sheet for the BGA2869 provides recommendations for PCB design such as ground planes, bias circuits, and input-output matching networks. You can refer to this information to design your own PCB. 

Hope these can help you.

(1) High Speed Layout Design Guidelines - NXP. https://www.nxp.com/docs/en/application-note/AN2536.pdf
(2) PCB design and layout guidelines for CBTU02044 - NXP. https://www.nxp.com/docs/en/application-note/AN12864.pdf
(3) AN3962, PCB Layout Design for Analog Applications - NXP. https://www.nxp.com/docs/en/application-note/AN3962.pdf

B.R.

Gavin

0 件の賞賛
返信