SDK Examples for Wireless MCUs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK Examples for Wireless MCUs

SDK Examples for Wireless MCUs

The wireless examples feature many common Bluetooth, zigbee and thread configurations. This article describes each SDK example. 

MCUs:

  • KW45
  • K32W1
  • KW47
  • MXCW71/72
Category SDK Example Name Description comments
BLE Controller hci_bb the HCI black box demo gives access to the BLE controller via serial interface using commands and events.   
Bluetooth adv_ext_central

the adv_ext_central implements a custom GATT based temperature Profile. After pairing with the peripheral, it configures notifications and displays temperature values on a terminal. 

Board to Board

Bluetooth

adv_ext_peripheral

the adv_ext_peripheral implements a custom GATT based temperature Profile. it begins with a general discoverable mode and waits for the central node to connect and configure notifications for the temperature value. 

Board to Board

Bluetooth

ancs_c

the demo acts as a peripheral that advertises a service solicitation for custom ANCS service. Also, can acts as a client once connected to the device offering the ANCS service. The application displays information about ANCS notifications received from the mobile. this service is available on iOS mobile devices.

 

Bluetooth

beacon

the demo has non-connectable advertising packets that are sent on the three advertising channels. From the info sent by the beacon we can see:

  • company identifier. 
  • beacon identifier. 
  • UUID, by default this value is a random value based on the UI of the board. 
  • some beacon application data 
  • RSSI

IoT toolbox app

Bluetooth

ble_fscibb

implements a custom GATT based wireless UART profile. it can be possible to interact with the device through a serial terminal.   

Serial Terminal 

Bluetooth

ble_shell

implements a console application that allows the user to interact with a full feature BLE stack library. implements GAP roles and both client and server, to enabling these roles can be done using some commands. this demo allows the user to add, erase or modify services. 

Serial Terminal

Bluetooth

eatt_central

the application behaves as a GAP central node. It scans for an EATT peripheral to connect to. Once connected it performs service discovery, initiates an EATT connection and configures indications on the peripheral for services A and B.  The central reports the received service data and steps taken during the setup on a serial terminal. 

Board to Board

Bluetooth

eatt_peripheral

the application behaves as a GAP peripheral node. it works a as general discoverable mode and waits for a GAP central node to connect. This application implements two services, Service A and Service B. After the EATT connection in completed, the peer must enable indications for the two services to periodically receive profile data over EATT.  

Board to Board

Bluetooth

hid_device

(Mouse) the demo moves the cursor in a square pattern between a min and max axis. this demo behaves as a GAP peripheral node with a general discoverable mode that waits for a GAP central node to connect. 

 

Bluetooth

hid_host

the application behaves as a GAP central node. it works as a GAP limited discovery Procedure and searches for HID devices to connect to. After connecting with the peripheral node, it configures notifications and displays the received HID reports on a serial terminal. 

Serial Terminal

Bluetooth

loc_reader

the application behaves as a GAP peripheral node. This application has the RASP profile implemented; it advertises for compatible devices, once it connected begins to send ranging data to the central device. 

Board to Board

Bluetooth

loc_user_device

the application behaves as a GAP central node. it scans for compatible devices, once it connected begins to send ranging commands to the peripheral device and calculates the distance estimation based on the information received. 

Board to Board

Bluetooth

otac_att

the over the air programming client is a GAP peripheral which advertising the BLE OTAP service and waits for a connection from an OTAP server. After an OTAP server connects, the OTAP client waits for it to write the OTAP control point CCCD and then starts sending commands via ATT indications. 

over the air programming tool //IoT toolbox app

Bluetooth

otac_I2cap

(different transfer method) The over the air programming client is a GAP peripheral which advertising the BLE OTAP service and waits for a connection from an OTAP server. After an OTAP server connects, the OTAP client waits for it to write the OTAP control point CCCD and then starts sending commands via ATT indications. 


over the air programming tool // IoT toolbox app

Bluetooth

otas

the Over the air programming server application is a GAP central which scans for devices advertising the BLE OTAP service. After it finds one, it connects to it and configures the OTAP control point CCC descriptor to receive ATT indications from the device then it waits fir OTAP commands from the device. 


over the air programming tool // IoT toolbox app

Bluetooth

temp_coll

the application behaves as a GAP central node, it enters GAP limited discovery procedure and searches for sensor devices to pair with. After pairing with the peripheral, it configures notifications and displays temperature values on a serial terminal. 

Board to Board

Bluetooth

temp_sens

the application behaves as a GAP peripheral node. it enters GAP general discoverable mode and waits for a GAP central node to connect and configure notifications for the temperature value. 

Board to Board

Bluetooth

w_uart

implements a custom GATT based wireless UART profile. it can be possible to interact with the device through a serial terminal. 

IoT toolbox app

Bluetooth

wireless_ranging

Is used to perform secure and highly accurate distance estimation between two BLE device. 

the application is made of two parts:

  • The embedded firmware, that can be controlled manually via serial connection.
  • the host application (python) running on a PC and controlling the firmware using serial link.

Wireless Ranging application allows to:

  • Configure most of the parameters required for measurement.
  • Select what type of measurement to be performed.
  •  Trigger CS measurements using range or test command.
  • Log system debug information but also raw IQ data information in MatLab.

Board to Board 

genfsk

connectivity_test

 

Board to Board

ieee_802.15.4

connectivity_test

 

Board to Board

reference design

bluetooth

this application is based on a GATT temperature Service and demonstrates power consumption optimization in BLE. The power consumption is optimized during advertising, connected and no activity states. 

 

无评分
版本历史
最后更新:
‎07-22-2025 08:08 AM
更新人: