Hello @nandan-khant ,
OK, understand your situation.
According to your above descripitons, these test plans didn't pass in WFA lab, Wi-Fi4, Wi-Fi5, SVD, FFD, WPA2SI, PMF, and WPA3-R2+R3.
Please follow thest steps to create ticket in our system FOR EACH test plan.
For example:
1. WPA3-R3 test plan
In Wi-Fi_CERTIFIED_WPA3_Test_Plan_v3.2, chaper "3.2.2 STAUT test applicability",
weidong_sun_3-1668738746845.png
if "STAUT SAE confirmation exchange variation test" failed, It will be better if you use 5.2.7_STAUT_SAE_ confirmation_exchange_variation_test named your log's file name.
......
2. Create a ticket via nxp website www.nxp.com
SUPPORT--->support ticket--->Create New Case
weidong_sun_0-1668737336020.png
weidong_sun_1-1668737377968.png
in your ticket, you should provide these information:
(1) Driver / Firmware version
(2) Android platfor information
(3) Hardware platform information
(4) Siniffer logs
(5) if you have ucc logs, provide it, please!
(6) wpa_supplicant version (the one in android 11 or from open source v2.10)
(As I am known, wpa_supplicant in android 11 doesn't support WPA3-R3, but in android 12, no problem)
(7) wpa_supplicant.conf
we need it's detailed configurations of wpa_supplicant.conf
Then I will share above information with internal team, and analyse it together.
Thanks!
Regards,
weidong