vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds

969 次查看
damodaranmurthy
Contributor I

vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds , after 10ms reinitialized and working fine. ADC read called for every one milliseconds,ADC config details: 12bit, ADIV/8, no low power , 16samples avg, normal speed , software trigger. ADC_init() called once at power up and later for ADC errors same ADC_init called again to reset.

0 项奖励
回复
1 回复

814 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Could you please specify which specific Vybrid part are you using? Additionally, are you using bare-metal code or any other BSP?

Best regards!

/Carlos

0 项奖励
回复