vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds

964 Views
damodaranmurthy
Contributor I

vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds , after 10ms reinitialized and working fine. ADC read called for every one milliseconds,ADC config details: 12bit, ADIV/8, no low power , 16samples avg, normal speed , software trigger. ADC_init() called once at power up and later for ADC errors same ADC_init called again to reset.

0 Kudos
Reply
1 Reply

809 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Could you please specify which specific Vybrid part are you using? Additionally, are you using bare-metal code or any other BSP?

Best regards!

/Carlos

0 Kudos
Reply