u-boot source code for EVB-VF522R3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot source code for EVB-VF522R3

ソリューションへジャンプ
4,883件の閲覧回数
kanoumamoru
Contributor III

Hi,

I am searching u-boot source code for EVB-VF522R3 board which has for the Vybrid-R VF522R automotive series.

Of cource, the SD card image is available via Freescale HP, but there is not a source code of u-boot.

I checked DENX u-boot source tree. I found out VF610TWR, but I could not find out VF522R3 contents.

Please let me know how to get u-boot code of EVB-VF522R3.

Best Regards,

kanou

ラベル(1)
タグ(2)
1 解決策
4,199件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Kanou,

Please refer to the attached patches. I noticed that both autoevb and twr are very similar. You just have to change the serial output to a different UART.

Of course you have to rebuild u-boot using the twr configuration.

Best Regards,

Alejandro

元の投稿で解決策を見る

8 返答(返信)
4,200件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Kanou,

Please refer to the attached patches. I noticed that both autoevb and twr are very similar. You just have to change the serial output to a different UART.

Of course you have to rebuild u-boot using the twr configuration.

Best Regards,

Alejandro

4,199件の閲覧回数
kanoumamoru
Contributor III

Great!  I'll try it.

Thanks.

kanou

0 件の賞賛
返信
4,199件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you take this case?

0 件の賞賛
返信
4,199件の閲覧回数
kanoumamoru
Contributor III

Hi Karina,

Unfortunately, Timesys support only TWR-VF65GS10 baord.

I can't find out EVB-VF522R3.

Thanks,

kanou

0 件の賞賛
返信
4,199件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ can you  help Kanou with this  question?

0 件の賞賛
返信
4,199件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Rene Kolarik can you comment please?

0 件の賞賛
返信
4,199件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano​ are you able to    help here?

0 件の賞賛
返信
4,199件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Karina,

I can delve into it. I will try to find something helpful.

Best Regards,

Alejandro