u-boot source code for EVB-VF522R3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot source code for EVB-VF522R3

Jump to solution
4,807 Views
kanoumamoru
Contributor III

Hi,

I am searching u-boot source code for EVB-VF522R3 board which has for the Vybrid-R VF522R automotive series.

Of cource, the SD card image is available via Freescale HP, but there is not a source code of u-boot.

I checked DENX u-boot source tree. I found out VF610TWR, but I could not find out VF522R3 contents.

Please let me know how to get u-boot code of EVB-VF522R3.

Best Regards,

kanou

Labels (1)
Tags (2)
1 Solution
4,123 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Kanou,

Please refer to the attached patches. I noticed that both autoevb and twr are very similar. You just have to change the serial output to a different UART.

Of course you have to rebuild u-boot using the twr configuration.

Best Regards,

Alejandro

View solution in original post

8 Replies
4,124 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Kanou,

Please refer to the attached patches. I noticed that both autoevb and twr are very similar. You just have to change the serial output to a different UART.

Of course you have to rebuild u-boot using the twr configuration.

Best Regards,

Alejandro

4,123 Views
kanoumamoru
Contributor III

Great!  I'll try it.

Thanks.

kanou

0 Kudos
Reply
4,123 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you take this case?

0 Kudos
Reply
4,123 Views
kanoumamoru
Contributor III

Hi Karina,

Unfortunately, Timesys support only TWR-VF65GS10 baord.

I can't find out EVB-VF522R3.

Thanks,

kanou

0 Kudos
Reply
4,123 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ can you  help Kanou with this  question?

0 Kudos
Reply
4,123 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Rene Kolarik can you comment please?

0 Kudos
Reply
4,123 Views
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano​ are you able to    help here?

0 Kudos
Reply
4,123 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Karina,

I can delve into it. I will try to find something helpful.

Best Regards,

Alejandro