u-boot source code for EVB-VF522R3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

u-boot source code for EVB-VF522R3

跳至解决方案
3,566 次查看
kanoumamoru
Contributor III

Hi,

I am searching u-boot source code for EVB-VF522R3 board which has for the Vybrid-R VF522R automotive series.

Of cource, the SD card image is available via Freescale HP, but there is not a source code of u-boot.

I checked DENX u-boot source tree. I found out VF610TWR, but I could not find out VF522R3 contents.

Please let me know how to get u-boot code of EVB-VF522R3.

Best Regards,

kanou

标签 (1)
标记 (2)
1 解答
2,882 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi Kanou,

Please refer to the attached patches. I noticed that both autoevb and twr are very similar. You just have to change the serial output to a different UART.

Of course you have to rebuild u-boot using the twr configuration.

Best Regards,

Alejandro

在原帖中查看解决方案

8 回复数
2,883 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi Kanou,

Please refer to the attached patches. I noticed that both autoevb and twr are very similar. You just have to change the serial output to a different UART.

Of course you have to rebuild u-boot using the twr configuration.

Best Regards,

Alejandro

2,882 次查看
kanoumamoru
Contributor III

Great!  I'll try it.

Thanks.

kanou

0 项奖励
回复
2,882 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you take this case?

0 项奖励
回复
2,882 次查看
kanoumamoru
Contributor III

Hi Karina,

Unfortunately, Timesys support only TWR-VF65GS10 baord.

I can't find out EVB-VF522R3.

Thanks,

kanou

0 项奖励
回复
2,882 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ can you  help Kanou with this  question?

0 项奖励
回复
2,882 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Rene Kolarik can you comment please?

0 项奖励
回复
2,882 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano​ are you able to    help here?

0 项奖励
回复
2,882 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi Karina,

I can delve into it. I will try to find something helpful.

Best Regards,

Alejandro