sample program of ADC,CAN.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

sample program of ADC,CAN.

跳至解决方案
1,431 次查看
soichiyamamoto
Contributor V

Hi,

My customer wants the sample program of the following peripheral.

・CAN

・ADC

I'm sorry, please give me a sample program of ADC,CAN.

Best Regards,

soichi

标签 (1)
0 项奖励
回复
1 解答
1,184 次查看
timesyssupport
Senior Contributor II

Hello Soichi,

We do not have a sample CAN application, as there is not currently CAN support with the Linux kernel/MQX for Vybrid Tower.

The MQX portion of the Vybrid Out of Box Experience Demo (OOBE Demo) uses the ADC. The sources are available from the MQX Installer, found here:

http://www.freescale.com/webapp/Download?colCode=FSLMQXOS_4_0_2_GA&appType=license&location=null&Par...

Please note, the ADC portion of this demo is commented out as it was previously not compatible with Linux. You can uncomment this code (lines 279-309 in FreescaleMQXRTOS4.0.2-GA/mcc/examples/oobe/ds5/oobe_twrvf65gs10_m4/Source/main_task.c ) when using the latest Linux kernel release by Timesys.

Build and runtime instructions can be found here:

https://linuxlink.timesys.com/docs/wiki/engineering/userguide_vybrid_mcc#Building-MQX

Thanks, and let me know if you have any questions.

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,185 次查看
timesyssupport
Senior Contributor II

Hello Soichi,

We do not have a sample CAN application, as there is not currently CAN support with the Linux kernel/MQX for Vybrid Tower.

The MQX portion of the Vybrid Out of Box Experience Demo (OOBE Demo) uses the ADC. The sources are available from the MQX Installer, found here:

http://www.freescale.com/webapp/Download?colCode=FSLMQXOS_4_0_2_GA&appType=license&location=null&Par...

Please note, the ADC portion of this demo is commented out as it was previously not compatible with Linux. You can uncomment this code (lines 279-309 in FreescaleMQXRTOS4.0.2-GA/mcc/examples/oobe/ds5/oobe_twrvf65gs10_m4/Source/main_task.c ) when using the latest Linux kernel release by Timesys.

Build and runtime instructions can be found here:

https://linuxlink.timesys.com/docs/wiki/engineering/userguide_vybrid_mcc#Building-MQX

Thanks, and let me know if you have any questions.

Timesys Support

0 项奖励
回复
1,184 次查看
naoumgitnik
Senior Contributor V

timesyssupport, may you help with it, please?

Thanks, Naoum Gitnik.

0 项奖励
回复