sample program of ADC,CAN.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sample program of ADC,CAN.

ソリューションへジャンプ
2,273件の閲覧回数
soichiyamamoto
Contributor V

Hi,

My customer wants the sample program of the following peripheral.

・CAN

・ADC

I'm sorry, please give me a sample program of ADC,CAN.

Best Regards,

soichi

ラベル(1)
0 件の賞賛
返信
1 解決策
2,026件の閲覧回数
timesyssupport
Senior Contributor II

Hello Soichi,

We do not have a sample CAN application, as there is not currently CAN support with the Linux kernel/MQX for Vybrid Tower.

The MQX portion of the Vybrid Out of Box Experience Demo (OOBE Demo) uses the ADC. The sources are available from the MQX Installer, found here:

http://www.freescale.com/webapp/Download?colCode=FSLMQXOS_4_0_2_GA&appType=license&location=null&Par...

Please note, the ADC portion of this demo is commented out as it was previously not compatible with Linux. You can uncomment this code (lines 279-309 in FreescaleMQXRTOS4.0.2-GA/mcc/examples/oobe/ds5/oobe_twrvf65gs10_m4/Source/main_task.c ) when using the latest Linux kernel release by Timesys.

Build and runtime instructions can be found here:

https://linuxlink.timesys.com/docs/wiki/engineering/userguide_vybrid_mcc#Building-MQX

Thanks, and let me know if you have any questions.

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,027件の閲覧回数
timesyssupport
Senior Contributor II

Hello Soichi,

We do not have a sample CAN application, as there is not currently CAN support with the Linux kernel/MQX for Vybrid Tower.

The MQX portion of the Vybrid Out of Box Experience Demo (OOBE Demo) uses the ADC. The sources are available from the MQX Installer, found here:

http://www.freescale.com/webapp/Download?colCode=FSLMQXOS_4_0_2_GA&appType=license&location=null&Par...

Please note, the ADC portion of this demo is commented out as it was previously not compatible with Linux. You can uncomment this code (lines 279-309 in FreescaleMQXRTOS4.0.2-GA/mcc/examples/oobe/ds5/oobe_twrvf65gs10_m4/Source/main_task.c ) when using the latest Linux kernel release by Timesys.

Build and runtime instructions can be found here:

https://linuxlink.timesys.com/docs/wiki/engineering/userguide_vybrid_mcc#Building-MQX

Thanks, and let me know if you have any questions.

Timesys Support

0 件の賞賛
返信
2,026件の閲覧回数
naoumgitnik
Senior Contributor V

timesyssupport, may you help with it, please?

Thanks, Naoum Gitnik.

0 件の賞賛
返信