mqxboot questions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mqxboot questions

跳至解决方案
2,530 次查看
Nouchi
Senior Contributor II

Hello,

I encounter difficulties to load and run M4 applications from linux with mqxboot. Applications works fine from debugger.

I build (successfully) and I tried mcc-pingpong demo without success (from timesys wiki).

From Timesys wiki the commande line is : mqxboot pingpong_example_twrvf65gs10_m4.bin 0x3f000000 0x3f000485

0x3f000000 is the load address in internal RAM, right?

and 0x3f000485 is the start address (odd address ???).

When I launch this, it crashes linux (have to hard reset).

Which address should I use ?

In the linker map file this line seems to interesting :

0x3f0004e0   0x00000068   Code   RO1055  * . text    psp.a(boot.o)

In this case 0x3f0004e0 seems to be the entry point.

If I try to launch mqxboot /home/demo-items/accelerometer_example_twrvf65gs10_m4.bin 0x3f000000 0x3f000485 (which is already build), it works.

Is there something to do with DS-5, it seems all things I build don't work.

I'm lost, somebody can help me.

Regards,

Emmanuel

Edit :

Now it works but :

- The Start address seems to be the Entry point address + 1

Somebody can explain why "+ 1" ?

1 解答
1,880 次查看
timesyssupport
Senior Contributor II

Hi Emmanuel,

The entry point I was referring to is defined at the top of the mapfile - at line 7 for me:

ARM Linker, 5.03 [Build 102]

=========================================================

Memory Map of the image

  Image Entry point : 0x3f0004e1

Section 19.11 in the Vybrid Reference manual specifies that the entry point should always be

odd because the Cortex-M4 supports only Thumb Mode - which I believe is why you needed to

add 1 to the other address you mention.

Thanks,

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,880 次查看
rendy
NXP Employee
NXP Employee

What version of MQX is it?

Btw. karinavalencia, I will on this, but isn't this question better suited for timesyssupport?

0 项奖励
回复
1,880 次查看
Nouchi
Senior Contributor II

Hello,

It's MQX 4.0.2. Now,  I can run MQX application from linux. I just like to know why start address must be Entry Point Address + 1.

In my case start address wasn't 0x3F0000485, because I compiled MQX with MQX_ROM_VECTORS 0, and I'm not ARM specialist (I'm a 68K old school man).

I don't find documents which explain how to use mqxboot.

Thanks,

Emmanuel

0 项奖励
回复
1,880 次查看
timesyssupport
Senior Contributor II

Hi Emmanuel,

To review, the usage of mqxboot is:

mqxboot <binary MQX image> <load address> <entry point>

You can find both the values of the load address and entry point in mapfile.map generated during the MQX image build. The entry point may not be 0x3f000485 if you have changed any MQX configuration options, so it is a good practice to verify the entry point in the mapfile.

Thanks,

Timesys Support

1,880 次查看
Nouchi
Senior Contributor II

Hello,

I understand how to use mqxboot, but why start address must be Entry Point address + 1?

0 项奖励
回复
1,881 次查看
timesyssupport
Senior Contributor II

Hi Emmanuel,

The entry point I was referring to is defined at the top of the mapfile - at line 7 for me:

ARM Linker, 5.03 [Build 102]

=========================================================

Memory Map of the image

  Image Entry point : 0x3f0004e1

Section 19.11 in the Vybrid Reference manual specifies that the entry point should always be

odd because the Cortex-M4 supports only Thumb Mode - which I believe is why you needed to

add 1 to the other address you mention.

Thanks,

Timesys Support

0 项奖励
回复
1,880 次查看
Nouchi
Senior Contributor II

hello,

This seems to be a good explanation.

Thanks,

Emmanuel

0 项奖励
回复
1,880 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you review this  case and share  your comments?

0 项奖励
回复