Dear Naoum,
That threat was for MQX, now we have a new project which needs to use linux. I compared registers control bit definitions between 8041 and 8081, almost all the same; I even found that 8081 chip is being used in Kinetis FRDM-K64 kit; downloaded the FSLMQX_FRDMK64 and checked the 8041 and 8081 C and Header files. They are also same line by line. I guess MII orRMII modes are selected in another .h file. Unfortunately we removed ethernet interface from project, therefore I could not test it.
Now we have another project, needs Ethernet interface.
Thanks for your helps again