Dear community,
I have a custom Vybrid VF3x prototype board, which has a Micrel KSZ8081 ethernet PHY chip. I have added the phy_KSZ8041 .c and .h files to my projects' BSP in order to add the ethernet interface. I am using KSZ8081 which is very similar to KSZ8041(8041 has bot MII and RMII modes) in RMII mode.
Therefore, If I set the KSZ8041 .c and .h files to RMII mode, may be it will be enough to start RTCS protocols.
Please help me how can I set the KSZ8041 into RMII mode?
Thanks and best regards.
Mehmet Ali Ipin.