What is TOTR in “Chapter 33 Cyclic Redundancy Check (CRC)” section of Vybrid Reference Manual?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is TOTR in “Chapter 33 Cyclic Redundancy Check (CRC)” section of Vybrid Reference Manual?

跳至解决方案
2,438 次查看
naoumgitnik
Senior Contributor V

On behalf of LilyZhang:

"It is present on the block diagram, but not mentioned on the register descriptions. May you comment on that, please?"

I'll look into it; it will take several days to clarify it.

Regards, Naoum Gitnik.

标签 (5)
0 项奖励
回复
1 解答
2,045 次查看
naoumgitnik
Senior Contributor V

On behalf of Lily Zhang:

Thanks for your help, Edward!

According to the reply from the Vybrid IC design team, "this feature is not used on Vybrid", and we will have to fix our documentation.

Regards, Naoum Gitnik.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,045 次查看
kef2
Senior Contributor V

Naoum,

DS-5 debugger shows TOT and TOTR bits defined in CRC_CTRL register. According to descriptions provided in DS-5 debugger registers view and according to Figure 33-1 in Vybrid RM Rev 5, these bits should control byte and/or bits transposition on input side (TOT) and output side (TOTR) of CRC block. According to DS-5 5.16, TOT are CTRL bits 31:30 and TOTR are CTRL bits 29:28.

I tried toggling TOT and TOTR bits in debugger but didn't notice any change in resulting CRC. I guess TOT and TOTR blocks are removed, at least in 1N02G maskset. It seems Figure 33-1 need an update.

BTW output registers are in low endian format, which is fine for me. Input requires byte reversal, TOT bits could help here.

IMO TCRC bit also could be removed. TCRC=0 is 16-bit mode, TCRC=1 is 32-bit mode. On 32-bit CPU I think it is much better to feed CRC unit with 4 bytes at once, even when calculating 16-bit CRC. See attached source for CRC16 CCIT (poly=1021).

2,046 次查看
naoumgitnik
Senior Contributor V

On behalf of Lily Zhang:

Thanks for your help, Edward!

According to the reply from the Vybrid IC design team, "this feature is not used on Vybrid", and we will have to fix our documentation.

Regards, Naoum Gitnik.

0 项奖励
回复