Vybrid input video signal when flicker noise has occurred.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid input video signal when flicker noise has occurred.

Jump to solution
2,383 Views
takashitakahash
Contributor III

Hi ncommunity.

Our customer has video signal flicker noise issues.

Input video signal to Vibrid When the video signal flicker has occurred.

Although I think that noise cause of the input signal, what  can reduce the noise by setting the register?

Also,  can I determine the effect by monitoring the value of the VDEC_NOISE?

Labels (1)
0 Kudos
Reply
1 Solution
2,052 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

Please rephrase your reply and add some details. 0.22uF works or not?

On reference board is used 0.1uF.

pastedImage_0.png

/Jiri

View solution in original post

9 Replies
2,052 Views
takashitakahash
Contributor III

Hellow Karina-san.

Customer  has been improved that noise issues showed that with a 0.22μF input coupling capacity.

The recommended value of the Vybrid reference board is 0.022μF.

It is not a problem even with a 0.22μF.

Input is the NTSC signal from the camera.

0 Kudos
Reply
2,053 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

Please rephrase your reply and add some details. 0.22uF works or not?

On reference board is used 0.1uF.

pastedImage_0.png

/Jiri

2,052 Views
takashitakahash
Contributor III

Customer using Integlity of GHS OS.

Hard ware is there own board.

Video signal is analog NTSC, it converting the built-in ADC to  the digital signal.

Symptoms is not a frame flicker, noise level (SN ratio) large, and  visible as noise is flickering.

0 Kudos
Reply
2,052 Views
karina_valencia
NXP Apps Support
NXP Apps Support

jiri-b36968​ can you continue with the follow up?

0 Kudos
Reply
2,052 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

Is the problem in video input signal or setting of the display is not correct?

Please add some details: Video of the issue, setting of VideoADC, parameters of the input signal and the noise, configuration of Vybrid, etc.

/Jiri

0 Kudos
Reply
2,052 Views
karina_valencia
NXP Apps Support
NXP Apps Support

takashitakahashi​ did you get previous comment?

0 Kudos
Reply
2,052 Views
timesyssupport
Senior Contributor II

Hello Takashi,

Can you describe your customer's hardware and OS configuration?

Is this a Vybrid VF5xx based design? Is Linux running on this hardware, or another OS?

How is the video signal input connected to the hardware?

Thank you,

Timesys Support

0 Kudos
Reply
2,052 Views
karina_valencia
NXP Apps Support
NXP Apps Support

takashitakahashi​ did you get previous comment?

0 Kudos
Reply
2,052 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you attend this case?

0 Kudos
Reply