Vybrid .icf linker command files: how to allow IAR debugger to access a port?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid .icf linker command files: how to allow IAR debugger to access a port?

跳至解决方案
2,526 次查看
kenmacfarlane
Contributor III

Getting  "Trying to read outside mapped memory at address:" when my code accesses a  port on the m4.

I have two apps, one which works properyl, is MQX based, and there

under project options linker config,.icf is in $TOOLKIT_DIR$\config\linker\Freescale\MVFxx_M4.icf.

I hacked a simple non-MQX one from a FSL 2D-ace demo, and it has a memory accession violation on the very first port access, using a .icf that looks similar (just has DDR added). 


There’s nothing in either .icf that  specifically allows the port address at 4000 0000, so does MQX allow it somehow, where non-MQX apps don't?

标签 (6)
标记 (1)
1 解答
2,210 次查看
kenmacfarlane
Contributor III

I spotted the problem - when you create a new workspace in IAR EWARM, the debugger is by default "Simulator" so every register access causes a memory access warning.

在原帖中查看解决方案

3 回复数
2,211 次查看
kenmacfarlane
Contributor III

I spotted the problem - when you create a new workspace in IAR EWARM, the debugger is by default "Simulator" so every register access causes a memory access warning.

2,210 次查看
rendy
NXP Employee
NXP Employee

Hi,

Which Vybrid do you use? I have VF6 reference manual on my table and the slot connected to 0x4000_0000 address is empty so accessing can fail. Nevertheless make sure you have properly initialized the peripheral you are accessing, mainly enabling the clock signal.

Rene

2,210 次查看
kenmacfarlane
Contributor III

Its a VF5, and the register (aka Port, but maybe I should have called it a register) was one of the CCM regs, just above CCM_BASE 0x4006B000, but the particular address didn't matter - the issue was the in debugger tab.

0 项奖励
回复