Vybrid VIU Up-scaling method.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid VIU Up-scaling method.

Jump to solution
1,680 Views
takashitakahash
Contributor III

Hi community.

Our customer has VIU Up-scaling method question.

Would you please answer tomorrow 23,Oct ,2015.

The description of 57.5.4.2 Up-scaling,

To achieve good display quality, progressive video input shall be used if down-scaling is needed.

It is described as but, what happens is what kind of events in the case of a progressive rather than interlaced input.

Example: the entire screen noise from entering or Jaggy noise  or Deterioration of the resolution etc.

Labels (1)
0 Kudos
Reply
1 Solution
1,507 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,508 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,508 Views
alfred_liu
NXP Employee
NXP Employee

Hi, takashitakahashi

I think we should follow the RM requirement at first, since the RM request the progressive input, certainly there are reasons or limitations for this.

the answer for your question is no meaning for your design.