Vybrid VIU Up-scaling method.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid VIU Up-scaling method.

跳至解决方案
1,759 次查看
takashitakahash
Contributor III

Hi community.

Our customer has VIU Up-scaling method question.

Would you please answer tomorrow 23,Oct ,2015.

The description of 57.5.4.2 Up-scaling,

To achieve good display quality, progressive video input shall be used if down-scaling is needed.

It is described as but, what happens is what kind of events in the case of a progressive rather than interlaced input.

Example: the entire screen noise from entering or Jaggy noise  or Deterioration of the resolution etc.

标签 (1)
0 项奖励
回复
1 解答
1,586 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,587 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
1,587 次查看
alfred_liu
NXP Employee
NXP Employee

Hi, takashitakahashi

I think we should follow the RM requirement at first, since the RM request the progressive input, certainly there are reasons or limitations for this.

the answer for your question is no meaning for your design.