Dear Ladies and Gentleman,
i am under review of the Vybrid Reference Manual F-Series to activate the flow controal for the UART-A.
In chapter 3.8.4.1 there is mentioned, that all uarts support Hardware flow control (RTS/CTS).
However, I did not find any more explanation how to use that feature?
Is there some documentation about that?
E.g. what are the relevant registers?
Many thanks
解決済! 解決策の投稿を見る。
So to add some explanation, the vybriddrm.pdf vybrid reference manual, rev 7, 06/2014 contains information in chapter 49.4.1.6 Hardware flow control.
Inside the vfxxx controller reference manual, rev. 0, 10/2016, i could not find that chapter about hardware flow control. Is it still possible to use the mechanism as mentioned in 49.4.1.6.?
So to add some explanation, the vybriddrm.pdf vybrid reference manual, rev 7, 06/2014 contains information in chapter 49.4.1.6 Hardware flow control.
Inside the vfxxx controller reference manual, rev. 0, 10/2016, i could not find that chapter about hardware flow control. Is it still possible to use the mechanism as mentioned in 49.4.1.6.?