Vybrid MCC in Linux without having M4 running

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid MCC in Linux without having M4 running

ソリューションへジャンプ
2,353件の閲覧回数
johannestraxler
Contributor III

Hello,

I have a program running in linux userspace which initializes MCC (mcc_initialize). The M4 core is not running, i.e. no image was loaded.

Additionally I create two endpoints. I experience that the program crashes after this operations!

Is this because there is no application running on M4?

Or can this error have any other reasons?

Currently I do not have the appropriate M4 application ready and as a starting point I just want to initialize the MCC and its endpoints from linux side. Data transfer will not be done!

Thanks,

Johannes

ラベル(2)
0 件の賞賛
返信
1 解決策
1,785件の閲覧回数
johannestraxler
Contributor III

I found out that the problem is not related to MCC or its drivers, but to stdout. When sending a special combination of character the program hangs and ends up with a SIGHUP linux signal.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,785件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 件の賞賛
返信
1,785件の閲覧回数
timesyssupport
Senior Contributor II

Hello Johannes,

Can you try running the following on the command-line before running your application:

# modprobe mcc

Thanks, and let me know how it goes.

Timesys Support

0 件の賞賛
返信
1,785件の閲覧回数
johannestraxler
Contributor III

Hi,

I loaded the kernel module everytime before starting the program, but this brings no improvement. Any other ideas?

(I'm using MCC version 1.0.3)

BR,

Johannes

0 件の賞賛
返信
1,785件の閲覧回数
timesyssupport
Senior Contributor II

Hello Johannes,

Another option would be to not load the mcc module before starting your application. mcc_initialize will not return MCC_SUCCESS. You can use an if statement on mcc_initialize() to check for this - if MCC_SUCCESS is not returned, do not create any endpoints or perform other MCC related actions.

Thanks,

Timesys Support

1,786件の閲覧回数
johannestraxler
Contributor III

I found out that the problem is not related to MCC or its drivers, but to stdout. When sending a special combination of character the program hangs and ends up with a SIGHUP linux signal.

0 件の賞賛
返信